FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Cables connected to the Ethernet port on the universal model QCPU
FAQ
Cables connected to the Ethernet port on the universal model QCPU
Which type of cable should I use for a connection to the Ethernet port on a universal model QCPU module, straight cable or cross cable?
- Category :
Answer
If a direct connection is made, either type can be used.
If making a connection via a hub, use a straight cable.
If making a connection via a hub, use a straight cable.
- Product Name
- MELSEC-Q Series
- Series
- Q (Q mode)