Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22692
  • Release Date : 2018/09/03 17:29
  • Update : 2018/10/03 16:23
  • Print

Input derating

What is input derating?
Category : 

Answer

Input derating is the percentage of simultaneous ON points, one of the specifications applied when input modules are used.
When QX42 is used in a temperature of 55 degrees Celsius and 28.8 VDC is applied, for example, the percentage of simultaneous ON points must be 40% or lower. For Q41X, the percentage must be 75% (24 out of 32 points) under the same condition.
Product Name
MELSEC-Q Series
Series
Input Module

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries