Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22712
  • Release Date : 2018/09/03 17:29
  • Print

Detecting the connection between a built-in Ethernet port QCPU and hub

How can I check the connection to a hub with a built-in Ethernet port QCPU?
Category : 

Answer

You can check the connection to the hub with bit 10 of the special register SD1288. When bit 10 of the SD1288 is on, the QCPU is in connection with the hub.
Product Name
MELSEC-Q Series
Series
Q (Q mode)
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?