Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22714
  • Release Date : 2018/09/03 17:29
  • Print

Boot file setting of the QnUDVCPU

Can I specify a memory card (SRAM card, ATA card, or Flash card) as the transfer source (boot source) of the boot file setting with the QnUDVCPU?
Category : 

Answer

No. You cannot use an SRAM card, ATA card, or Flash card. Specify an SD memory card as the transfer source (boot source).
Product Name
MELSEC-Q Series
Series
Q (Q mode)
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?