FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-Q Series > Hardware setting for using Q series extension base units
FAQ
Hardware setting for using Q series extension base units
Do I need to configure any hardware setting to use Q series extension base units?
- Category :
Answer
You need to set the number of extension base units with the connector for setting the number of extension base units.
For details, refer to the following.
SH-080473 QCPU User's Manual (Hardware Design, Maintenance and Inspection)
4.3 Connecting an Extension Base Unit
For details, refer to the following.
SH-080473 QCPU User's Manual (Hardware Design, Maintenance and Inspection)
4.3 Connecting an Extension Base Unit
- Product Name
- MELSEC-Q Series
- Series
- CPU