FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > QnA-compatible 3E frame command for built-in Ethernet port in LCPU
FAQ
QnA-compatible 3E frame command for built-in Ethernet port in LCPU
An error C059h is returned when I use a multiple-block batch read command (0406) for the QnA-compatible 3E frame of the MC protocol in the built-in Ethernet port in the L series CPU. What is the remedy?
- Category :
Answer
The built-in Ethernet port in the L series CPU is not compatible with a multiple-block batch read command (0406) of the MC protocol. Executable commands are the following.
- Batch read: 0401
- Batch write: 1401
- Random read: 0403
- Test (random write): 1402
- Monitor registration: 0801
- Monitor: 0802
- Remote password unlock: 1630
- Remote password lock: 1631
- Batch read: 0401
- Batch write: 1401
- Random read: 0403
- Test (random write): 1402
- Monitor registration: 0801
- Monitor: 0802
- Remote password unlock: 1630
- Remote password lock: 1631
- Product Name
- MELSEC-L Series
- Series
- L Series