FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Boot operation from the standard ROM
FAQ
Boot operation from the standard ROM
Is it possible to boot LCPU from the standard ROM?
- Category :
Answer
The boot operation from the standard ROM is not possible.
The program memory of LCPU is a flash ROM.
Thus, writing in the program memory achieves a ROM operation.
The program memory of LCPU is a flash ROM.
Thus, writing in the program memory achieves a ROM operation.
- Product Name
- MELSEC-L Series
- Series
- CPU