Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22731
  • Release Date : 2018/09/03 17:29
  • Print

Use of an A-compatible 1E frame for the built-in Ethernet port of LCPU

Can I use an A-compatible 1E frame of the MC protocol for the built-in Ethernet port in the L series CPU?
Category : 

Answer

The built-in Ethernet port in the L series is compatible only with a QnA-compatible 3E frame of the MC protocol. An A-compatible 1E frame is not supported.
Product Name
MELSEC-L Series
Series
L Series
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?