FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Battery replacement for LCPU
FAQ
Battery replacement for LCPU
Are contents of the program memory, the standard RAM, and latch devices erased when the battery of LCPU is replaced?
- Category :
Answer
The contents of the standard RAM and latch devices are not erased if the battery replacement is completed within three minutes, which is the backup power time.
Since the program memory is a flash ROM, the data is not erased even if the battery runs down.
Since the program memory is a flash ROM, the data is not erased even if the battery runs down.
- Product Name
- MELSEC-L Series
- Series
- CPU