Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22737
  • Release Date : 2018/09/03 17:29
  • Print

Simple PLC communication function

What is the simple PLC communication function?
Category : 

Answer

This function allows data communications between specified devices at the specified timing, using the built-in Ethernet.
Device data such as production data can be transferred without a program just by doing simple settings from a programming too.
Furthermore, this function allows for easy communication not only between the L series devices, but also with existing systems that use the Q series and QnA/A series. The target modules are CPU modules whose first 5 digits of the serial number are "13042" or later.
Product Name
MELSEC-L Series
Series
CPU

May I have your opinion?

Inquiries