FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > NTP support by the SNTP function of LCPU with built-in Ethernet port
FAQ
NTP support by the SNTP function of LCPU with built-in Ethernet port
Is it possible to use a personal computer NTP server as an SNTP server for the time setting function (SNTP client) via the built-in Ethernet port in the L series CPU?
- Category :
Answer
NTP and SNTP are compatible. Therefore, an NTP server can be used for clock setting.
- Product Name
- MELSEC-L Series
- Series
- L Series