FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Retention of auto tuning setting value for temperature control module
FAQ
Retention of auto tuning setting value for temperature control module
Is it possible to retain the auto tuning setting value of the temperature control module L60TCTT4BW after the power is turned OFF?
- Category :
Answer
Use the automatic backup setting.
While "1: enabled" is set in the CH[] automatic backup setting after auto tuning of PID constants in the buffer memory (Un\G63, Un\G95, Un\G127, Un\G159), the buffer memory data can be automatically backed up in the non-volatile memory when auto tuning is done.
While "1: enabled" is set in the CH[] automatic backup setting after auto tuning of PID constants in the buffer memory (Un\G63, Un\G95, Un\G127, Un\G159), the buffer memory data can be automatically backed up in the non-volatile memory when auto tuning is done.
- Product Name
- MELSEC-L Series
- Series
- L Series