Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22806
  • Release Date : 2018/09/03 17:30
  • Print

LCPU built-in I/O function

What function does LCPU built-in I/O function provide?
Is it possible to use it for general-purpose I/O function or high-speed counter function?
Category : 

Answer

The built-in I/O functions are standard functions of the L series CPU. Combining these functions flexibly achieves various controls with lower cost, eliminating the need for dedicated modules for each function.
The output type of the built-in I/O (function) is selectable between sink type and source type.
For more details, refer to "MELSEC-L CPU Module User's Manual (Built-In I/O Function)".
Product Name
MELSEC-L Series
Series
CPU

May I have your opinion?

Inquiries