Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22810
  • Release Date : 2018/09/03 17:30
  • Print

LCPU protection function

Can I set a password to protect LCPU programs so that it acts like a black box?
Category : 

Answer

A password can be set.
- Use the file password 32 function.
- Number of characters: 4 to 32 (alphanumeric and special characters, case-sensitive)
- Disabled operations: Write, read, read/write
- Target: Programs (program files), parameters, device comments, initial device values, symbolic information
Product Name
MELSEC-L Series
Series
CPU
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?