FAQ


FAQAbout Products
 
 - FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > LCPU protection function
FAQ
LCPU protection function
      Can I set a password to protect LCPU programs so that it acts like a black box?
    
  - Category :
Answer
    A password can be set. 
- Use the file password 32 function.
- Number of characters: 4 to 32 (alphanumeric and special characters, case-sensitive)
- Disabled operations: Write, read, read/write
- Target: Programs (program files), parameters, device comments, initial device values, symbolic information
    - Use the file password 32 function.
- Number of characters: 4 to 32 (alphanumeric and special characters, case-sensitive)
- Disabled operations: Write, read, read/write
- Target: Programs (program files), parameters, device comments, initial device values, symbolic information
- Product Name
- MELSEC-L Series
- Series
- CPU