FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > L60AD4 accuracy
FAQ
L60AD4 accuracy
What is the accuracy of L60AD4?
- Category :
Answer
- Ambient temperature: 25+/-5 degrees Celsius with tolerance of +/-0.1%
- Ambient temperature: 0 to 55 degrees Celsius with tolerance of +/-0.2%
(Accuracy for the maximum digital output value.)
- Ambient temperature: 0 to 55 degrees Celsius with tolerance of +/-0.2%
(Accuracy for the maximum digital output value.)
- Product Name
- MELSEC-L Series
- Series
- A / D Conversion Module