Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22813
  • Release Date : 2018/09/03 17:30
  • Print

Maximum number of modules to be connected to L26CPU-(P)BT

What is the maximum number of modules connectable to L26CPU-(P)BT?
Category : 

Answer

Up to 40 modules.
When the branch module and extension module are used, use L26CPU-(P)BT CPU modules whose first 5 digits of the serial number are "13072" or later.
Product Name
MELSEC-L Series
Series
L Series

May I have your opinion?

Inquiries