Start main contents

Factory Automation

  • Font Size
  • S
  • M
  • L

Questions

  • No : 22815
  • Release Date : 2018/09/03 17:30
  • Print

Use of END cover with the branch module and extension module

Are there any restrictions on the END cover when the L series branch module and extension module are used?
Category : 

Answer

Use an END cover applicable to the following.
- The L6EC whose serial number (first six digits) is "*****2" or later
- END cover with ERR terminal (optional item)
Product Name
MELSEC-L Series
Series
Other Modules (terminal block, connector, cable etc.)
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?