FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > CPU operation when the time setting failed
FAQ
CPU operation when the time setting failed
Does a CPU error stop to occur when the time setting via the built-in Ethernet port on an LCPU module is made and a specified SNTP server does not operate?
- Category :
Answer
When an error occurs, the operation can be stopped or continued according to the "At Error Occurrence" setting.
(The default is "Continue".)
(The default is "Continue".)
- Product Name
- MELSEC-L Series
- Series
- CPU