FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC-L Series > Error code "2110" in LCPU
FAQ
Error code "2110" in LCPU
The error code "2110" has occurred in LCPU. Are there any remedies?
- Category :
Answer
The error code "2110" is "SP.UNIT ERROR.". This error may be caused by one of the following factors.
(1) The module that has been specified by a FROM/TO instruction is not an intelligent function module.
(2) The module that has been specified by a FROM/TO instruction does not have buffer memory.
(3) The intelligent function module that a FROM/TO instruction has specified as an access target is out of order.
The FROM/TO instruction that has caused the error can be specified using the error jump of the diagnostics function (PLC diagnostics) provided by the programming tool, GX Developer or GX Works2.
(1) The module that has been specified by a FROM/TO instruction is not an intelligent function module.
(2) The module that has been specified by a FROM/TO instruction does not have buffer memory.
(3) The intelligent function module that a FROM/TO instruction has specified as an access target is out of order.
The FROM/TO instruction that has caused the error can be specified using the error jump of the diagnostics function (PLC diagnostics) provided by the programming tool, GX Developer or GX Works2.
- Product Name
- MELSEC-L Series
- Series
- CPU