FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > Statements of GX Works2 and the scan time
FAQ
Statements of GX Works2 and the scan time
Does the scan time change when statements are displayed in the Navigation window of GX Works2?
- Category :
Answer
The input method for statements, either "PLC" or "Peripheral", makes a difference.
- If "PLC" is set for statements, they are written into the program memory.
The string [Title], necessary for display in the project view, is also written to the program memory thus increasing
the number of steps.
-> The increase in the steps slightly affect the scan time.
*The scan time is increased by Increase in steps × NOP processing time
*The increase in steps is 3 to 4(It depends on the number of bytes of the statements.).
- If "Peripheral" is set for statements The display of statements in the project view does not affect the scan time
(The addition of the string [Title] does not increase the number of steps.).
- If "PLC" is set for statements, they are written into the program memory.
The string [Title], necessary for display in the project view, is also written to the program memory thus increasing
the number of steps.
-> The increase in the steps slightly affect the scan time.
*The scan time is increased by Increase in steps × NOP processing time
*The increase in steps is 3 to 4(It depends on the number of bytes of the statements.).
- If "Peripheral" is set for statements The display of statements in the project view does not affect the scan time
(The addition of the string [Title] does not increase the number of steps.).
- Product Name
- Engineering Software, MELSEC-Q Series, MELSEC-L Series
- Series
- Software Package (GPP function), CPU, MELSEC-L Series