FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > Switch settings of intelligent function module and I/O assignment settings (GX Works2)
FAQ
Switch settings of intelligent function module and I/O assignment settings (GX Works2)
In GX Works2, both intelligent function module settings and the I/O assignment setting have switch settings. Which one should I set?
- Category :
Answer
Those switch settings are connected with each other. The switch setting of intelligent function module settings are easier to set.
- Product Name
- Engineering Software
- Series
- Software Package (GPP function)