Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22934
  • Release Date : 2018/09/03 17:30
  • Update : 2018/09/25 09:49
  • Print

Time out error in the communication test of MX Component

When I use MX Component, a time out error occurs in the communication test with an Ethernet interface module. What is the cause of this error?
Category : 

Answer

The possible causes are as follows.
 -  Incorrect setting with a personal computer or an Ethernet interface module
    Check the IP address, network number, station number, and other settings.
 - Improper condition of the HUB or LAN cable
    Check the connection of the LAN cable or the HUB for the power discontinuity.
 - Incorrect setting of the communication setting utility
    Check if the settings of the Ethernet interface module and the settings of the communication setting utility match.
Product Name
Engineering Software
Series
Middleware

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries