FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > Device numbers set in the initial setting procedure registration window of the CC-Link remote device station
FAQ
Device numbers set in the initial setting procedure registration window of the CC-Link remote device station
Do I have to change device numbers of Initial data processing request flag (RX18) and others for each station number in the initial setting procedure registration window of the remote device station?
- Category :
Answer
You do not have to change the device numbers for each station number in the initial setting procedure registration window.
Example) When the AJ65SBT2B-64AD has been connected to the station numbers 1 and 2 In the initial setting procedure
registration window, set RX18 for Initial data processing request flag of both the station numbers 1 and 2.
Example) When the AJ65SBT2B-64AD has been connected to the station numbers 1 and 2 In the initial setting procedure
registration window, set RX18 for Initial data processing request flag of both the station numbers 1 and 2.
- Product Name
- Engineering Software
- Series
- Software Package (GPP function)