Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22954
  • Release Date : 2018/09/03 17:30
  • Print

An error (error code: F1028) occurs when compilation is executed in GX Works2.

I have created a program "with labels" with GX Works2, and an error (error code: F1028) occurs when I execute compilation (conversion).
Category : 

Answer

You have used the device set as the automatic assignment device for labels in the program. Change the device with the one out of the range or change the automatic assignment device range.
Product Name
Engineering Software
Series
GX Works2

May I have your opinion?

Inquiries