FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > I cannot select [Transfer Setup] in GX Developer because it is displayed in gray.
FAQ
I cannot select [Transfer Setup] in GX Developer because it is displayed in gray.
When I attempted to change the connection destination by selecting [Transfer Setup] of [Online] from the tool bar to start the communication between a programmable controller and GX Developer, [Transfer Setup] has been displayed in gray and I was not able to select it.
- Category :
Answer
You cannot select the item while the programmable controller is being monitored.
Execute [Close all windows] of [Window] from the tool bar, and check if Transfer Setup can be selected.
Execute [Close all windows] of [Window] from the tool bar, and check if Transfer Setup can be selected.
- Product Name
- Engineering Software
- Series
- GX Developer