Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 22958
  • Release Date : 2018/09/03 17:31
  • Print

I cannot convert a circuit created with GX Developer.

When I create a program and execute (operate) the conversion with GX Developer in the offline status (No programmable controller has been connected), a communication error message is displayed and the program is not converted.
Category : 

Answer

When the conversion is executed, online change is automatically executed.

When the online change at the upper right section of the setting in "Options" of "Tools" from the GX Developer tool bar has been set to "After conversion, Write during RUN", change it to "After conversion, Don't write to PLC".
Product Name
Engineering Software
Series
GX Developer

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries