FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Difference between QJ61BT11 and QJ61BT11N
FAQ
Difference between QJ61BT11 and QJ61BT11N
What are the differences between QJ61BT11 and QJ61BT11N?
- Category :
Answer
QJ61BT11N supports Version 2 (expanded cyclic setting), the setting for refreshing/forced clearing a slave station data when the switch on a programmable controller CPU is set to STOP, and other functions.
For more details, refer to the following manual.
- CC-Link System Master/Local Module User's Manual
Appendix 5 Difference from traditional modules
Appendix 5.2 Precautions when replacing a QJ61BT11 with a QJ61BT11N
For more details, refer to the following manual.
- CC-Link System Master/Local Module User's Manual
Appendix 5 Difference from traditional modules
Appendix 5.2 Precautions when replacing a QJ61BT11 with a QJ61BT11N
- Product Name
- Network Related Products
- Series
- CC-Link