Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23012
  • Release Date : 2018/09/03 17:31
  • Print

Connecting the CC-Link IE Field Network with a personal computer

Can I use a commercial personal computer as one of CC-Link IE Field Network stations if the computer has the 1000BASE-T port on it and the port is directly connected?
Category : 

Answer

To pursue high speeds, the CC-Link IE Field Network applies a communication control method different from that applied to the Ethernet communication for personal computers. Hence a personal computer cannot be directly connected to the CC-Link IE Field Network. Connect the computer to the Network via the Ethernet adapter module NZ2GF-ETB.
Product Name
Network Related Products
Series
CC-Link IE Field Network
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?