Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23013
  • Release Date : 2018/09/03 17:31
  • Print

Difference between networks called CC-Link and those called MELSEC

What are the differences between the CC-Link IE Field Network or CC-Link IE Controller Network, a network with its name including CC-Link, and the MELSECNET/H or MELSECNET/10 network, a network with its name including MELSEC?
Category : 

Answer

CC-Link IE, supported by the CC-Link Partner Association, is an open field network standard that integrates networks, from a controller network to field/motion networks, into a single Ethernet-based network.

MELSECNET/H and MELSECNET/10 are networks specific to the MELSEC programmable controllers. There are two types of networks: the PLC to PLC network that provides communication between controllers and the remote I/O network that provides communication with remote I/O stations.
Product Name
Network Related Products
Series
CC-Link IE Field Network
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?