Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23021
  • Release Date : 2018/09/03 17:31
  • Print

CC-Link signals checked when an error occurs

Which input signals of the CC-Link master module do I need to check when a CC-Link error occurs?
Category : 

Answer

Check the following signals.
- Module error signal : X0
- Host data link status signal: X1
- Other station data link status signal: X3
Product Name
Network Related Products
Series
CC-Link
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?