Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23030
  • Release Date : 2018/09/03 17:31
  • Update : 2018/09/26 10:17
  • Print

How to make the expanded cyclic setting for CC-Link local stations

How do I make the expanded cyclic setting for a CC-Link local station?
Category : 

Answer

Make the expanded cyclic setting for a CC-Link local station using the programming tool, GX Developer or GX Works2. Follow the procedure below.

(1) Set the CC-Link Network Parameter setting "Mode" to "Remote Net(Ver.2 Mode)" or "Remote Net(Additional Mode)"
      for the local station.
(2) Select "Operation Setting" and make "Expanded Cyclic Setting" in the "Operation Setting" window.
Product Name
Network Related Products
Series
CC-Link
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?