FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Unit of the receive data length used by the QJ71C24N series pre-defined protocol support function
FAQ
Unit of the receive data length used by the QJ71C24N series pre-defined protocol support function
If "Non-conversion Variable" is selected for the packet setting of the QJ71C24N series pre-defined protocol support function, which one is the unit of the receive data length of the variable, byte or word?
- Category :
Answer
The receive data length of the variable is specified in bytes.
- Product Name
- Network Related Products
- Series
- Computer Link / Serial Communication
May I have your opinion?
Related FAQ
- Receiving data when no receive complete code is designated (QJ71C24N)
- Connecting QJ71C24N to an external device that has no DTR signal
- Difference between AJ65SBTB1-16DT and AJ65SBTB1-16DT1
- Assigning X and Y signals of AJ65SBTB1-32DT
- Limitation on the number of levels of cascade connections when QJ71E71-100 is used