FAQ
![](/usr/file/attachment/q&a.jpg)
![](/usr/file/attachment/q&a_sp.jpg)
FAQAbout Products
![](/usr/file/attachment/img_mv-1_sm.jpg)
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Unit of the receive data length used by the QJ71C24N series pre-defined protocol support function
FAQ
Unit of the receive data length used by the QJ71C24N series pre-defined protocol support function
If "Non-conversion Variable" is selected for the packet setting of the QJ71C24N series pre-defined protocol support function, which one is the unit of the receive data length of the variable, byte or word?
- Category :
Answer
The receive data length of the variable is specified in bytes.
- Product Name
- Network Related Products
- Series
- Computer Link / Serial Communication