Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 23040
  • Release Date : 2018/09/03 17:31
  • Print

Limitation on the number of levels of cascade connections when QJ71E71-100 is used

Is there limitation on the number of levels of cascade connections when QJ71E71-100 is used?
Category : 

Answer

If a repeater hub is used, 10BASE-T allows a maximum of four levels of cascade connections and 100BASE-TX allows a maximum of two levels of cascade connections. Ask the manufacturer about the allowable number of levels when using a switching hub.
Product Name
Network Related Products
Series
Ethernet Interface Module

May I have your opinion?

Inquiries