Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23041
  • Release Date : 2018/09/03 17:31
  • Print

Order in which a CC-Link master module and slave stations are connected

Is it possible to establish a CC-Link network in which a master station is positioned in the center and slave stations are connected at both right and left hand sides of the master module?
Category : 

Answer

There is no restriction on the positions of a master station and slave stations where they are connected. (Stations are not required to be connected in order of station number.) Hence connections can be made in a way that puts a master station in the center.
Product Name
Network Related Products
Series
CC-Link
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?