Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23042
  • Release Date : 2018/09/03 17:31
  • Print

Whether or not multiple QJ72LP25-25 modules can be mounted

Is it possible to mount two QJ72LP25-25 modules in a MELSECNET/H remote I/O station?
Category : 

Answer

No, only a single QJ72LP25-25 can be mounted (and is to be mounted on the CPU slot on a main base unit).
Product Name
Network Related Products
Series
MELSECNET/H
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?