FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Duplication error in a CC-Link master station
FAQ
Duplication error in a CC-Link master station
When a CC-Link master station is started, the master station duplication error with the code BBC5H occurs. What causes the error?
- Category :
Answer
Possible causes are as follows.
(1) Another master station exists on the same line.
(2) Noise is detected on the line at power on.
(1) Another master station exists on the same line.
(2) Noise is detected on the line at power on.
- Product Name
- Network Related Products
- Series
- CC-Link