FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Link data from communication error stations in a CC-Link network
FAQ
Link data from communication error stations in a CC-Link network
What becomes of the data received from a communication error station that occurs during a CC-Link data link?
- Category :
Answer
The remote input RX of the master station and the remote input RX and remote output RY of local stations clear/hold the data from an error station according to the corresponding setting.
The remote register RWr of the master station and the remote register RWw and RWr of local stations hold the data from an error station whichever the setting is.
The remote register RWr of the master station and the remote register RWw and RWr of local stations hold the data from an error station whichever the setting is.
- Product Name
- Network Related Products
- Series
- CC-Link