Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23063
  • Release Date : 2018/09/03 17:31
  • Print

Limitation on the number of MELSOFT products that can be connected with the QJ71E71

What is the maximum number of the MELSOFT products I can connect with the QJ71E71 series?
Category : 

Answer

In the TCP/IP connection, you can connect up to 17 MELSOFT products at the same time using a dedicated connection for system and the connections for users 1 to 16. In the UDP/IP communication, you can connect multiple MELSOFT products and GOTs using a dedicated connection for system.
Product Name
Network Related Products
Series
Ethernet Interface Module
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?