FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Limitation on the number of MELSOFT products that can be connected with the QJ71E71
FAQ
Limitation on the number of MELSOFT products that can be connected with the QJ71E71
What is the maximum number of the MELSOFT products I can connect with the QJ71E71 series?
- Category :
Answer
In the TCP/IP connection, you can connect up to 17 MELSOFT products at the same time using a dedicated connection for system and the connections for users 1 to 16. In the UDP/IP communication, you can connect multiple MELSOFT products and GOTs using a dedicated connection for system.
- Product Name
- Network Related Products
- Series
- Ethernet Interface Module