FAQ


FAQAbout Products

- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Assignment for connecting two CC-Link remote input modules (16-point type) (Remote net Ver.1 mode)
FAQ
Assignment for connecting two CC-Link remote input modules (16-point type) (Remote net Ver.1 mode)
When I have connected two CC-Link remote input modules (16-point type) and set the remote input refresh device to "X100" in the remote net Ver.1 mode, what will the assignment of X devices be for each station?
- Category :
Answer
X devices will be assigned as follows. (With this setting, 32 points are occupied per station.)
- Station No. 1: X100 to X11F
- Station No. 2: X120 to X13F
The first 16 points of each station are used by a program.
- Station No. 1: X100 to X11F
- Station No. 2: X120 to X13F
The first 16 points of each station are used by a program.
- Product Name
- Network Related Products
- Series
- CC-Link