Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23083
  • Release Date : 2018/09/03 17:31
  • Update : 2018/09/26 13:16
  • Print

Differences between the AJ65SBTB1-16TE and AJ65SBTB1B-16TE1

What are the differences between the AJ65SBTB1-16TE and AJ65SBTB1B-16TE1? 
Category : 

Answer

The following shows the major differences.

- AJ65SBTB1-16TE
  - 1-wire terminal block, 1-common type
  - Maximum load current: 0.1 A/point
  - Protection functions (overload protection, overheat protection) are provided.

 - AJ65SBTB1B-16TE1
   - 1-wire terminal block, 2-common type
   - Maximum load current: 0.5 A/point
   - No protection function

For details, refer to the following.
 - Open Field Network CC-Link Compatible Product Catalog
Product Name
Network Related Products
Series
CC-Link
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?