FAQ


FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Network related products > Differences between the AJ65SBTB1-16TE and AJ65SBTB1B-16TE1
FAQ
Differences between the AJ65SBTB1-16TE and AJ65SBTB1B-16TE1
What are the differences between the AJ65SBTB1-16TE and AJ65SBTB1B-16TE1?
- Category :
Answer
The following shows the major differences.
- AJ65SBTB1-16TE
- 1-wire terminal block, 1-common type
- Maximum load current: 0.1 A/point
- Protection functions (overload protection, overheat protection) are provided.
- AJ65SBTB1B-16TE1
- 1-wire terminal block, 2-common type
- Maximum load current: 0.5 A/point
- No protection function
For details, refer to the following.
- Open Field Network CC-Link Compatible Product Catalog
- AJ65SBTB1-16TE
- 1-wire terminal block, 1-common type
- Maximum load current: 0.1 A/point
- Protection functions (overload protection, overheat protection) are provided.
- AJ65SBTB1B-16TE1
- 1-wire terminal block, 2-common type
- Maximum load current: 0.5 A/point
- No protection function
For details, refer to the following.
- Open Field Network CC-Link Compatible Product Catalog
- Product Name
- Network Related Products
- Series
- CC-Link