FAQ


FAQAbout Products
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nHCPU > Speed limit value
FAQ
Speed limit value
When the speed limit value is changed, does that change affect a command speed lower than the speed limit value?
- Category :
-
- FAQ > Controllers > Motion Controllers > MELSEC iQ-R Series > Motion Controllers > RnMTCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nDSCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nDCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q170MSCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q170MCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nHCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nCPUN
Answer
No, there is no impact on the command speed.
However, the actual acceleration/deceleration time are affected by the change.
However, the actual acceleration/deceleration time are affected by the change.
- Product Name
- Motion controller
- Series
- MELSEC iQ-R
MELSEC-Q