Start main contents

  • Font Size
  • S
  • M
  • L

Questions

  • No : 23562
  • Release Date : 2018/09/14 15:09
  • Print

Major error 093CH

What is major error 093CH?
What should I do when it occurs?
Category : 

Answer

Major error 093CH occurs when the absolute position is erased.
Execute the home position return after checking the batteries of the Motion CPU module and the servo amplifier.
Product Name
Motion controller
Series
MELSEC iQ-R
Did you solve your question?

If it is not resolved please ask from here.

Contact Us

May I have your opinion?