FAQ


FAQAbout Products
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nDCPU > Servo amplifier forced stop
FAQ
Servo amplifier forced stop
How do I disable the forced stop of servo amplifiers?
- Category :
-
- FAQ > Controllers > Motion Controllers > MELSEC iQ-R Series > Motion Controllers > RnMTCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nDSCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nDCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q170MSCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q170MCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nHCPU
- FAQ > Controllers > Motion Controllers > MELSEC-Q Series > Motion Controllers > Q17nCPUN
Answer
Set "[PA04] Function selection A-1" to "_1_ _h: Invalid".
(Note): When using Q17nCPUN, set "Servo amplifier parameter 23
(Optional function 1)" to "0001".
(Note): When using Q17nCPUN, set "Servo amplifier parameter 23
(Optional function 1)" to "0001".
- Product Name
- Motion controller
- Series
- MELSEC iQ-R
MELSEC-Q