FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > Engineering Software > Externally switching the operating status of a programmable controller
FAQ
Externally switching the operating status of a programmable controller
How can I externally switch the operating status of a programmable controller?
Answer
On the Project view of the Navigation window, select "Parameter" → "PLC Parameter" using GX Works2 (or GX Developer). Click the "PLC System(1)" tab, and set the "RUN Terminal Input".
Connect a switch to the RUN terminal set in parameter and transfer program/parameters from the personal computer to the programmable controller. Then, the operating status can be changed using the switch connected.
To enable the RUN/STOP operation by using the switch connected, keep the RUN/STOP switch of a programmable controller in the STOP position.
Connect a switch to the RUN terminal set in parameter and transfer program/parameters from the personal computer to the programmable controller. Then, the operating status can be changed using the switch connected.
To enable the RUN/STOP operation by using the switch connected, keep the RUN/STOP switch of a programmable controller in the STOP position.
- Product Name
- FX1S, FX1N, FX1NC, FX3S, FX3G, FX3GC, FX2N, FX2NC, FX3U, FX3UC
- Product Category
- Main unit, Engineering Software, GX Works2, GX Developer
- Series
- MELSEC-F series
May I have your opinion?
Related FAQ
- How to check the version of the MELSEC-F series
- Built-in variable analog potentiometers of the FX3G series
- How to change the keeping (latched device data) range (FX3G/FX3GC)
- Necessity of a battery when a memory cassette is used
- Connecting a USB interface of a personal computer to a programmable controller