FAQ
FAQAbout Products
- FAQ > Controllers > Programmable Controllers MELSEC > MELSEC iQ-F Series > CPU Module > Regarding the difference of current address (user unit, pulse unit)
FAQ
Regarding the difference of current address (user unit, pulse unit)
What is the difference between a current address (user unit) and a current address (pulse unit)?
Answer
The difference between the current address (user unit) and the current address (pulse unit) is as follows:
The current address (user unit) becomes the unit system (motor system/mechanical system/composite system) and is filled with a value that does not include the position data magnification.
The current address (pulse unit) is the motor system unit and includes the position data magnification.
The current address (user unit) becomes the unit system (motor system/mechanical system/composite system) and is filled with a value that does not include the position data magnification.
The current address (pulse unit) is the motor system unit and includes the position data magnification.
- Product Name
- FX5U, FX5UC, FX5UJ, FX5S
- Product Category
- CPU Module, Motion/Positioning
- Series
- MELSEC iQ-F Series