Start main contents

Factory Automation

FAQ

Factory Automation

FAQAbout Products

  • Font Size
  • S
  • M
  • L
  • No : 39363
  • Release Date : 2023/02/15 13:04
  • Print

Regarding differences between 8 bit and 16 bit modes for non-protocol communication

Please tell me how to use 8 bit mode and 16 bit mode when using non-protocol  communication.
Category : 

Answer

In 8-bit mode, the upper 8 bits of transmitted and received data are ignored and only the lower 8 bits are valid data.
In 16 bit mode, send/receive data is divided into lower and upper 8 bits.
If the external device you want to communicate with sends and receives data in 8-bit units, you can also set the PLC to 8-bit mode so that there is no need to divide the received data after sending and receiving.
Product Name
FX5U, FX5UC, FX5UJ, FX5S
Product Category
CPU Module, Network/Communication
Series
MELSEC iQ-F Series

May I have your opinion?

Please provide your feedback below. This is for feedback only. You will not receive a response.

Inquiries